Point Operation Discrepancy Time under range

The
Point Operation Discrepancy Time
value is less than the minimum allowed. Enter a value from 10 through 65530 in increments of 10, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal