Output Error Latch Time over range

The
Output Error Latch Time
value is greater than the maximum allowed. Enter a value from 0 through 65530, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal