Invalid Point Mode
Point Operation Type
is set to Equivalent
or
Complementary
for a pair of points and one of the Point
Mode
value is Standard
, creating an invalid
combination.Set
Point Mode
to a valid combination and apply the changes.Provide Feedback