Search
1732 EtherNet Safety Discrete
Input Delay Time under range
The
Input Delay Time
value is less than the minimum allowed. Enter a value from 0 through 126 in increments of 6, and then apply the changes.
Troubleshooting
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal