Test Outputs view parameters

Parameter
Description
Point
Indicates the number of the point to which the configuration is applied.
Point Mode
Specifies the mode for each point. Valid values include:
  • Not Used
    (default). The test output point is not used.
  • Standard
    . The test output point is configured as a standard output.
  • Pulse Test
    . The test output point is configured as a test output.
  • Power Supply
    . The test output point is configured as a power supply output.
  • Muting Lamp
    . The test output point is configured as a muting output. This option is only available for Point 03 and Point 07.
Point Mode
appears shaded in Run mode or when the project is safety secured.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal