Outputs view parameters

Parameter
Description
Point
Indicates the number of the point to which the configuration is applied.
Point Operation Type
Specifies how a pair of points is evaluated. Valid values include:
  • Single
    . Each point is evaluated individually.
  • Dual
    . Points are evaluated as a pair (Normally Open/Normally Open or Normally Closed/Normally Closed).
Point Operation Type
appears shaded in Run mode or when the project is safety secured.
Point Mode
Specifies a mode for each output point. Valid values include:
  • Not Used
    (default). The output point is not used.
  • Safety Pulse Test
    . The output point is used with a test pulse.
  • Safety
    . The output point is used without a test pulse.
Point Mode
appears shaded in Run mode or when the project is safety secured.
Output Error Latch Time
Specifies the minimum time a Safety Output error is latched.
Valid values are from 0 ms through 65530 ms in increments of 10 ms. The default is 1000 ms.
Output Error Latch Time
appears shaded in Run mode or when the project is safety secured.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal