Alarms view parameters
The
Alarms
view includes these parameters:Parameter | Description |
|---|---|
Disable All Alarms | Prevents the device from generating any of the four process alarms (LL, L, H, and HH) or the rate alarm and does not allow access to any of the alarm configuration properties. |
High High Limit | Sets the trigger point in Engineering Units. HHAlarm is set to 1 when the input signal moves above this limit. |
High Limit | Sets the trigger point in Engineering Units. HAlarm is set to 1 when the input signal moves above this limit. |
Low Limit | Sets the trigger point in Engineering Units. LAlarm is set to 1 when the input signal moves below this limit. The Low Alarm Limit must be >/= the Low Low Limit and < the High Limit. |
Low Low Limit | Sets the trigger point in Engineering Units. LLAlarm is set to 1 when the input signal moves below this limit. The Low Alarm Limit must be greater than or equal to the Low Low Limit and less than the High Limit. |
Deadband | Allows the process alarm status bits to remain set, even if the alarm condition disappears, as long as the channel data remains within plus or minus the deadband value of the process alarm. This Deadband value is entered in Engineering Units . |
Provide Feedback