Modbus Configuration

Modbus Configuration Summary
The Modbus section allows the user to change the Filter's Modbus Settings. When changing the device's Modbus settings, the user will select apply and save settings after configuring. Afterward, the user must reset the board by selecting "Reset PQconnect.” This tab configures the device address, baud rate, and parity mode. One thing to note is that the slave address, baud rate, and parity settings must be the same on both the PQvision Desktop and the device for the communication to work via PQvision desktop.
Slave Address:
Allows customers to choose which Filter’s PQconnect board they are communicating with.
Baud Rate:
Baud rate is the speed of communication. The default value is 115200.
Parity:
A parity bit is used for error detection. The default setting is even.
Save Settings
Saves any modified settings so that they will remain after a power cycle. Saving the settings will automatically open the contactor.
Reset PQconnect
This is an easy and effective way to power cycle the Filter’s PQconnect board. Any unsaved settings will be lost. If the Modbus settings are changed, the user must reset them.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal