Status/Diagnostics

Module diagnostics provide information on a module-wide basis. For example, the Module Diagnostics dialog box indicates the mode within which a module is operating, that is, Run, Remote Run, Remote Program, or Program. For more information about diagnostics, refer to Compact 5000 I/O Digital Modules documentation, PN 5069-UM004:
Refer to RA publication "Compact 5000 I/O Digital Modules documentation, PN 5069-UM004", available for download at the Rockwell Automation website (www.rockwellautomation.com) for detailed information on status, diagnostics, error codes, and alarms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal