Function
The Compact 5000™ 5069-IV16F-SC and 5069-IV16FK-SC are 16-Point, 12/24 VDC fast digital source input modules designed to expand the local I/O capability of Rockwell Automation Compact 5000™ Systems. K versions of the module are conformally coated.
The module is designed to interface by wiring an input pin to a switch so that the controller can detect either an open or a closed switch position. The inputs are IEC 61121-2, Type 3 inputs and therefore can also convert resistance placed across the input. It is also possible to interpret voltage present at the input as a switch. This means the inputs are able to operate with an analog signal and digitize that signal based on the specification limits for an input to be either an open or closed switch.
Provide Feedback