Certifications

Certifications for this module normally include UL, CSA (Class I, Div 2, Groups ABCD), and CE. Refer to the markings on the module side label and to the specifications in the Owner’s Guide for more detailed information and other compliance marks. Products with a CE mark are approved for installation within the European Union and EEA regions. Products with a UKCA mark are approved for installation within England and Scotland. The CE and UKCA Declarations of Conformance (DoC files) for this module are available from Spectrum Controls.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal