Communication
5069 Backplane Communication
- Connected producer/consumer multicast IO communication.
- Settable RPI (0.2 to 750.0 ms).
- Support for multiple controllers, either "Listen Only" or multiple owners. Multiple owners requires a Device Definition configuration of Connection = Data, Counters = None, and Input Data = Data or Packed Data.
- Local chassis operation, or Remote chassis operation (over CIP network).
- Unconnected messaging from controller (MSG instruction) or from a CIP network client. Typical uses include Reset or Reconfigure the module.
NOTE:
Refer to detailed protocols and MSG examples described in the module’s "User’s Manual."Provide Feedback