Sample Projects

The RSLogix5000 ladder logic Sample Projects for the 1756sc-CTR8 module demonstrate how to perform auxiliary functions, such as Reset, Reconfigure, or Unlatch alarms, in addition to synchronous copy of data to or from user-defined tags. Synchronous copy would be used with the AOP when "block integrity” of the data is needed (see "Data” section above).
NOTE
: The original Sample Projects for this module used the 1756 Generic Module profile. Please check the "SC website” for updated Sample Projects which use this custom Add-on-Profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal