Documentation
The primary source for detailed information about this module is the Spectrum Controls document, "Owner’s Guide 0300199-01”, referred to throughout this document as the "Owner’s Guide”, and sometimes called an "Operations Manual”. Available for download from the "SC website” are:
- "Owner’s Guide”, Technical Notes, Revision Notes, FAQ
- Presentations, Application stories
- Sample Projects, EDS files, Firmware Updates, etc.
EDS File
The EDS file is used for identifying the module to network tools, such as RSNetWorx or a CIP (refer to "CIP” in RSLogix5000 HELP) network browser (e.g. RSLinx Who). The EDS file can be downloaded from the "SC website” and installed using the RSLinx Hardware Installation Tool.
Certifications
Certifications for this module normally include CSA and FM (Class I, Div 2, Groups ABCD), plus UL and CE. Refer to the markings on the module side label and to the specifications in the Owner’s Guide for a more detailed information. Products with a CE mark are approved for installation within the European Union and EEA regions. The CE Declaration of Conformance (DOC file) for this module is available from Spectrum Controls.
Provide Feedback