Documentation

Downloads

The primary source for detailed information about this module is the ILX56-PND User Manual. Available for download from the ProSoft Technology, Inc. web site at www.prosoft-technology.com are:
  • User Manual and Datasheet
  • Presentations, Application stories and setup videos may also be available
  • Add-On Profile, EDS file, GSDML file, PLX50 Configuration Utility, etc.

GSDML File

The GSDML file contains the necessary device parameters required to correctly configure the device for data exchange in the PROFINET network. The GSDML file can be downloaded from the ProSoft Technology, Inc. website at www.prosoft-technology.com.

EDS File

The EDS file is used for identifying the module to network tools, such as RSNetWorx or a CIP (refer to “CIP” in RSLogix5000 HELP) network browser (e.g., RSLinx Who). The EDS file can be downloaded from the ProSoft Technology, Inc. website at www.prosoft-technology.com, and installed using the RSLinx Hardware Installation Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal