Documentation

Manual
The primary sources for detailed information about this module are the following documents available from www.mt.com/SLP85xD :
  • SLP85xD User Manual
  • Standard Automation Interface - Reference Manual
  • SLP85xD Intallation Manual
EDS File
The EDS file is used for identifying the module to network tools, such as RSNetWorx or a CIP (refer to "CIP" in RSLogix5000 HELP) network browser (e.g. RSLinx Who). The EDS file can be retrieved from the SLP85xD Documentation CD, or from the internet at www.mt.com/SLP85xD (Device Description - SLP85xD - EIP) and installed using the EDS Hardware Installation Tool for RSLinx. PLEASE NOTE: The SLP85xD's EDS file should NOT be loaded into STUDIO5000 to be used as an AOP module. This custom AOP should be used for that purpose instead.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal