Application Configuration
Configuration Assembly
(class 0x4, instance 5, attribute 3)
The configuration assembly consists of two parts. "Config Inputs" and the "Config
Outputs".
Config Inputs
(class 0x4, instance 100, attribute 3)
Configuration of the input assembly
48 configurable inputs can be set to the following input data values:
- Off
- Analog x Instantaneous value (x = 1 - 40)
- Analog x Totalizer (x = 1 - 40)
- Digital x State (x = 1 - 20)
- Digital x Totalizer (x = 1 - 20)
- Math x Process value (x = 1 - 12)
- Math x Totalizer (x = 1 - 12)
Config Outputs
(class 0x4, instance 150, attribute 3)
Configuration of the output assembly
48 configurable outputs can be set to the following output values:
- Off
- Analog x Instantaneous value (x = 1 - 40)
- Digital x State (x = 1 - 20)
Provide Feedback