Additional Device Information
Device Name
(class 0x01, instance 1, attribute 7)
Individual device name.
Device Tag
(class 0x315, instance 1, attribute 4)
Individual device tag.
SW Version
(class 0x315, instance 1, attribute 1)
Software version of the device.
Order Code
(class 0x315, instance 1, attribute 2)
You can order identical hardware with this code. This code changes on account of changes to
the hardware and you can enter the new code you received from the manufacturer here.
Serial Number
(class 0x315, instance 1, attribute 3)
Via the serial number you can obtain further device data or documentation from the Internet
or from your responsible sales office.

Provide Feedback