System Units
Corrected Volume Flow Unit
Select corrected volume flow unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Nl/h *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Corrected Volume Unit
Select corrected volume unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Nm³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Density Unit
Select density unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg/l *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Mass Flow Unit
Select mass flow unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg/h *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Mass Unit
Select mass unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Reference Density Unit
Select reference density unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg/Nl *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Temperature Unit
Select temperature unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | °C *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Volume Flow Unit
Select volume flow unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | l/h *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Volume Unit
Select volume unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | m³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Pressure Unit
Select process pressure unit
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | bar *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Water Density Unit
Select unit for the density of the water
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg/m³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Water Reference Density Unit
Select unit for reference density of the water
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | kg/Nm³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Provide Feedback