General

Designated Use

The measuring device described in these Operating Instructions is to be used only for measuring the mass flow rate of liquids and gases. At the same time, the system also measures fluid density and fluid temperature. These parameters are then used to calculate other variables such as volume flow. Fluids with widely differing properties can be measured.
Examples:
  • Chocolate, condensed milk, liquid sugar
  • Oils, fats
  • Acids, alkalis, lacquers, paints, solvents and cleaning agents
  • Pharmaceuticals, catalysts, inhibitors
  • Suspensions
  • Gases, liquefied gases, etc.
Resulting from incorrect use or from use other than that designated the operational safety of the measuring devices can be suspended. The manufacturer accepts no liability for damages being produced from this.

Connection versions

The measuring device can be connected to the EtherNet/IP network in one of three ways. Refer to the “Supplementary Documentation” for information on how to connect the device to an EtherNet/IP network.

Measuring device

The measuring device has an Ethernet module to connect it to an EtherNet/IP network and for connecting to the integrated Webserver. It uses the EtherNet/IP communication protocol (Ethernet Industrial Protocol) in accordance with the ODVA specification.

Data

The main measuring values are transmitted via EtherNet/IP communication. The sequence of the input and output values can be configured via the local display as well as via the integrated Webserver. Refer to the “Supplementary Documentation” for further information.

Communication

EtherNet/IP Network
  • Ethernet switch settings
  • 10 or 100Mbps
  • The default IP and MAC addresses are printed on the connections nameplate
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal