Petroleum
API commodity group
Select API commodity group of the measured medium
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | A - crude oil *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
API table selection
Select reference density by API table
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | API table 53/54 *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Oil density sample
Enter the value for the oil density of the sample
Property | Value |
|---|---|
Selection / Range | 470 - 1210 kg/m³ |
Factory Setting | 850 kg/m³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Oil pressure sample
Enter value for the oil pressure of the sample
Property | Value |
|---|---|
Selection / Range | 0 - 1.4e+16 bar |
Factory Setting | 1.01325 bar *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Oil temperature sample
Enter value for the oil temperature of the sample
Property | Value |
|---|---|
Selection / Range | -273.15 - 99726.8499 °C |
Factory Setting | 15 °C *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Petroleum mode
Select petroleum mode
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Off *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
S&W input mode
Select input mode for sediment and water
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Off *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Thermal expansion coefficient
Enter the thermal expansion coefficient of the measured medium
Property | Value |
|---|---|
Selection / Range | 414e-6 - 1674e-6 1/K |
Factory Setting | 414e-6 1/K *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Water cut mode
Select water cut mode
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Calculated value *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Water density sample
Enter value for the water density of the sample
Property | Value |
|---|---|
Selection / Range | 900 - 1200 kg/m³ |
Factory Setting | 999.2 kg/m³ *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Water temperature sample
Enter value for the water temperature of the sample
Property | Value |
|---|---|
Selection / Range | -273.15 - 99726.8499 °C |
Factory Setting | 15 °C *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Provide Feedback