Medium Selection
Select medium
Select medium type
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Liquid *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Select gas type
Select measured gas type
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Methane CH4 *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Reference sound velocity
Enter sound velocity of gas at 0 °C (32 °F)
Property | Value |
|---|---|
Selection / Range | 1 - 99999.9999 m/s |
Factory Setting | 415.0 m/s *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | FLOAT |
Calculation model
Select a formula for the temperature compensation of viscosity
Property | Value |
|---|---|
Selection / Range |
|
Factory Setting | Polynomial *Depends on order options or device settings |
Visibility | Operator |
Write Access | Maintenance |
Data Type | ENUM16 |
Provide Feedback