Liquistation CSFxx Overview
This overview section provides quick access to a list of the main module functions, some
attributes, and the location of more detailed module information.
IMPORTANT:
When developing an application, or troubleshooting
a significant problem, it is IMPORTANT to read and follow more detailed module information,
including safety recommendations. The primary source of detailed module information is the
Liquiline CA80x EtherNet/IP manual available from the Endress+Hauser website (www.endress.com).
Provide Feedback