Configuration Parameters
Webserver Enable
(class 0x310, instance 1, attribute 3)
Use this parameter to enable or disable access to the webserver in the device. If you
cannot reach the webserver, please check first whether the device is reachable over the
network using the "ping" command. If you cannot reach the device using the
"ping" command, please contact your networt administrator to check whether the
network is configured correctly and an IP-route to the device webserver exists.
Value | Webserver enable |
|---|---|
0 | ON |
1 | OFF |
Open Configuration
Press this button to open the configuration webpage of the device with your default
webbrowser.
The webbrowser will load a javascript application which allows remote operation of the
device display. During remote operation the local operation is temporarily disabled to
prevent simultaneous changes to the device parameterization. The local operater can retake
the operation anytime from the webbrowser.
Open Logbooks (*.dat)
Press this button to open a webpage with your default webbrowser, which contains URL links
to different logbooks in *.dat file format. These files can be imported into the Field Data
Manager software available from Endress+Hauser.
Open Logbooks (*.csv)
Press this button to open a webpage with your default webbrowser, which contains URL links
to the logbooks in *.csv file format. You can save these files to disk and open it with any
text editor.
Provide Feedback