Volume & Mass Totalizer Control
Totalizers can be reset to 0.
Once the Reset button is pressed the corresponding totalizer will be immediately reset to
0.
In the PLC program, a preset value can also be set via the acyclic communication. Thus, the
totalizer can be set to a certain value that is not equal to 0. The addresses can be found in
the fieldbus description manual.
Provide Feedback