Device Web Server

The FLOWave 8098 has a webserver. This is useful for viewing operation data remotely.
With Ethernet/IP the IP address of the device upon delivery is 192.168.0.100. The IP address can be changed with the display of FLOWave if available.

Logging Onto the Web Server

On the home page, click on Login on the top left.
Enter your user name and password:
  • User name: admin
  • Password: current device password
Click on Login.

Password

The device factory password is dependent on the specific device. It can be either "admin" or printed on the device itself. If the password is "admin". It is recommended to change the password for security reasons.
Changing passwords
  • Log in to the webserver.
  • Enter and confirm the new password in the menu General Settings.
Reset passwords to factory settings
  • Click on Login.
  • On the bottom right of the login window, click on Reset passwords.
  • The device must be rebooted within 3 minutes so that the passwords can actually be reset. A restart can be triggered via the FLOWave display, the Bürkert Communicator software or via a voltage reset.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal