Density
Damping
The damping makes it possible to damp the fluctuations of the measured values of the liquid
density:
- on the display,
- on the PLC input.
The damping of the liquid density comes in addition to the damping set for the mass flow
rate.
The damping is not applied to the new measured value if the 2 following conditions are met:
- a Low, Medium or High damping level is active,
- and the variation between 2 values that are measured one after the other is higher than 30 % (for example when charging the pipe or stopping the flow).
By default, the measured liquid density values are damped with the level Medium.
Damping level | Response time |
|---|---|
None |
|
Low | 1 s |
Medium | 10 s |
High | 30 s |
Mode
Density mode can be selected through the following values.
Mode | Density value calculation |
|---|---|
Measured | Value measured via SAW signals, and liquid temperature |
Water | Value calculated based on liquid temperature measured by FLOWave |
Constant | Value set to a constant value |
Linear | r = a+bT; coefficients a and b to be set by installer, T in °C |
Quadratic | r = a+bT+cT 2 ; coefficients a, b and c to be set by installer, T in
°C |
Provide Feedback