Troubleshooting

Status/Diagnostics
Refer to the 3401 Manual (see information under the "Documentation” topic) for a detailed list of the module’s status bits.
Refer to the 3401 Manual, and or the Add On Profile Indicator LED Help topic, for a detailed list of the module’s LEDs.
Additional Troubleshooting assistance in the form of FAQs can be downloaded from the Tech Library section of the AMCI website (hotlink on AOP Vendor tab).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal