Sample Projects
Sample programs are available for download from the Tech Library section of the AMCI website at www.amci.com
Sample programs for the 3401 and 3401L modules are available using used both the Add On Profiles and the 1734 Generic Module Profile (1734-MODULE).
Provide Feedback