Indicators and LEDs
The LED’s on the front panel allow you to quickly verify the operating status of the module. The Module LED tells you the status of the module, The Network Status LED indicates the state of the network connection, and the Limit Input and Home Input LEDs indicate that the discrete input is active.
- Module LED
- Solid Green:Module is OK with no motion in progress
- Blinking Green:Module is OK with motion occurring
- Blinking Red:Configuration Error, Command Error, Input Error, Home Invalid Error, or an Invalid Profile Error
- Network Status
- OFF: No Communication with scanner module
- Green: Communicaitng with scanner module
- Red: Communication Error
- Limit and Home Inputs
- OFF: Input is not active
- Orange: Input is active
- These LEDs will be ON if the Input has been configured as Active High and is receiving power or if the Input has been configured as Active Low and is not receiveing power.
Provide Feedback