Documentation
Manuals, Sample Programs, and Add On Instructions
The manual, sample programs, and Add On Instructions for the AMCI 3401 and 3401L CompactLogix modules can be downloaded from the AMCI website (hotlink on AOP Vendor tab).
CE Conformance
A CE declaration of conformance (DOC) file is available from AMCI on request.
Provide Feedback