Support

Website
www.amci.com (hotlink on AOP Vendor tab).
Contacts
Please contact AMCI for Technical Support regarding this RSLogix 5000 profile, the module itself, or any Sample Project. A list of distributors is on the AMCI website, as well as Technical Support, in the form of documents and FAQs. 24 Hour technical support is also available at 860-583-7271 during business hours (8AM - 5PM EST). At other times, an automated system will take your message and page an engineer on call. Please have your product model number and a description of the problem ready before you call.
Email: techsupport@amci.com
Tel: 860.583.7271 (24 Hour support)
Firmware Updates
Please contact AMCI Technical Support (above).
Module Repair and Replacement Options
Call AMCI at 860-585-1254 for a Return Merchandise Authorization number with model and serial numbers and a description of the problem.
NOTE: Proper handling precautions must be used to avoid damage from Electrostatic Discharge.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal