Documentation
Manuals
Manuals for both the AMCI 1241 and 1242 ControlLogix modules can be downloaded from the AMCI website (hotlink on AOP Vendor tab).
EDS File
An EDS file is used for identifying the module to network devices, such as a CIP network browser (e.g. RSLinx Who or RSNetworx). It is not needed for module operation. No EDS files are currently available for these modules.
CE Conformance
A CE declaration of conformance (DOC) file is available from AMCI on request.
Provide Feedback