Physical device does not match module configured in project

The physical device does not match the configured device in the project. These parameters must match for the physical device to match the configured device:
  • Vendor
  • Product Type and Product Code for a particular Vendor's catalog number
  • Major Revision
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal