DANGER - Connection Interruption
Resetting this device interrupts the connection to the device. Do not reset a device
currently used for control. Resetting the device interrupts the connection to the device, to
any device connected through this device, and from other controllers.
- SelectYesto reset the device.
- SelectNoto cancel this operation.
- SelectHelpfor more information.
Provide Feedback