Reset a device
Use
Reset
to emulate the cycling of power.
IMPORTANT:
Resetting the device interrupts the connection to the device and to any other device that
is connected through it. Connections from other controllers may be interrupted as well.
Ensure a connection interruption at this time is acceptable before proceeding. You should
not interrupt the connection on a device that is currently being used for control.
To reset a device
- On the tab for the device where you are updating information, selectReset.
- In the apply changes dialog box, selectYes.
Provide Feedback