Number of configured axes exceeds maximum axes count
Unsuccessful attempt to change the device. The device cannot change when the number of
configured axes exceeds the maximum number of axes in the device.
Select
OK
to return to the Change type
dialog
box.Provide Feedback