Mismatched EDS condition detected

A mismatched EDS condition was detected; the registered EDS file does not match the EDS file used to create the imported device.
To correct the problem:
  • If the currently registered EDS file is incorrect, register the EDS file that was registered when the device was created.
  • If the currently registered EDS file is correct, the device was skipped during import. Recreate the device using the currently registered EDS file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal