Failed to modify properties

You attempted to use an axis with a device that has time synchronization set up inappropriately.
To update the properties
  1. Open the 1756-ENxTx communication device properties.
  2. In the
    Overview
    view, select
    Device definition
    .
  3. In
    Device definition
    , set
    Time Sync Connection
    to
    Time Sync and Motion
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal