Error setting the chassis size
Error setting the chassis size. The error message indicates one of these conditions. Reenter
the chassis size and select
Apply
.Chassis size invalid
The size of the chassis in invalid.
Failed to reduce the size of a chassis
You cannot set chassis size to a size that is less than the last device in the chassis.
Provide Feedback