Increased CPU processing speeds and memory in new terminals are supported in Connected Components Workbench software Release 8.0
MILWAUKEE, March 9, 2015 — Rockwell Automation reduces boot-up time and increases installation flexibility with the new space-saving Allen-Bradley PanelView 800 family of graphic terminals.
The terminals, available in 4-inch, 7-inch and 10-inch display sizes, feature an 800 MHz CPU processor, up to 256 MB of flash, and dynamic memory to reduce boot-up time, making it two times faster than the previous PanelView Component terminal. The terminals also offer improved touch-screen responsiveness and can be configured in portrait and standard landscape mode for greater installation flexibility.
“The PanelView 800 family of terminals builds on the Rockwell Automation Connected Components Workbench software’s value of giving machine builders simplified engineering, easy configuration, faster installation and reduced start-up time,” said Chee Wah Lee, product manager, Rockwell Automation. “This family of graphic terminals is ideally suited for meeting control and visualization requirements in a wide range of simple, standalone applications, such as pump stations, packaging machines, labelers and stretch-wrap machines.”
The PanelView 800 graphic terminals are specifically designed for use with the Allen‑Bradley Micro800 and MicroLogix control systems. The terminals’ high-resolution screens with LED backlights can display up to 65,536 colors, providing a sharp display for a wide range of applications. Built-in Ethernet and serial communications ports (RS232, RS422 and RS485) support easier controller connectivity, while USB and microSD ports make file transfers easier. The terminals are also certified for Class 1, Division 2 hazardous locations.
The Connected Components Workbench software Release 8.0, which includes support for the PanelView 800 graphic terminals, gives machine builders a common environment to program the Micro800 controllers, as well as to configure the Allen-Bradley PowerFlex drives and Allen-Bradley Guardmaster safety relays.
The standard edition is free, and Release 8.0 includes support for the Guardmaster 440C-CR30 safety relay Ethernet plug-in for communications to Micro800 and Allen-Bradley CompactLogix controllers; the Micro800 high-speed counter plug-in feedback axis to ease motion programming; and Micro800 DeviceNet scanner plug-in diagnostics to ease troubleshooting DeviceNet-connected devices.
Users can also purchase the developer edition, which includes an archive manager to track the project with a timestamp and description, making device management easier. The developer edition also offers an enhanced Micro800 programming experience, with intellectual property protection, user-defined data types, a spy list to monitor variables easier, and the ability to make program logic changes while in run mode.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Sandra Sim
Rockwell Automation
65.6622.5131
ssim@ra.rockwell.com
Beatrice Zvosec
PadillaCRT
612.455.1914
beatrice.zvosec@padillacrt.com
Allen-Bradley, CompactLogix, Connected Components Workbench, Guardmaster, LISTEN. THINK. SOLVE., Micro800, MicroLogix, PanelView and PowerFlex are trademarks of Rockwell Automation Inc.
DeviceNet is a trademark of ODVA Inc.
Published March 8, 2015