Loading
Press Release | July 30, 2015
Recent ActivityRecent Activity

Process Engineers Save 50 Percent in Hardware Footprint With New AADvance Eurocard System

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

New system is one of the first process safety systems designed for use in subsea applications

MILWAUKEE, July 30, 2015 — Process engineers can reduce their physical hardware footprint by 50 percent using the new AADvance Eurocard process safety system from Rockwell Automation. The new system is ideally suited for industry applications with more restrictive physical space requirements, such as subsea control platforms. It is one of the first process safety systems designed for use in these highly demanding applications.

“The AADvance Eurocard system is our answer to customer feedback and an industry need for better integration in space-restrictive applications,” said Allan Rentcome, global technology director for Systems and Solutions at Rockwell Automation. “With the smaller system, process engineers can save equipment real estate and still achieve up to 500 I/O per controller. Users also have the option to scale up to meet the size of the standard AADvance system.”

The AADvance Eurocard system helps enable companies to protect people, equipment and the environment by achieving safe and continuous operation, and reducing the risk of human error. The system allows users to control and update their plantwide safety management systems from a single workstation, helping reduce the time spent updating individual terminals and margin for human error.

Sharing the same controller platform, workbench software, process modules, firmware and electronics as the traditional AADvance platform, the AADvance Eurocard system can be custom configured to meet different levels of safety (nonsafety to SIL 3) and each user’s specific system requirements. The system is specifically designed for functional safety and critical control applications, providing a flexible, scalable, distributed solution for a wide range of process industries.

The system is certified by Exida for functional safety and adheres to the latest safety standards. The system meets the functional safety requirements for Safety Integrity Level 3 (SIL 3) and is compliant with IEC 61508: 2010, Parts 1-7.

News Release Assets
Image available upon request or here at box.com.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.

Media Contacts
Marilyn Muscenti
Rockwell Automation
440.646.4087
memuscenti@ra.rockwell.com

Molly O’Mara
PadillaCRT
612.455.1918
molly.omara@padillacrt.com

AADvance and LISTEN. THINK. SOLVE. are trademarks of Rockwell Automation Inc.

Published July 29, 2015


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Process Engineers Save 50 Percent in Hardware Footprint With New AADvance Eurocard System