Loading
Press Release | January 30, 2020
Recent ActivityRecent Activity

New PUR and PVC Single-Cable Options Ease Installation, Maintenance

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Industrial operators can speed up installation times and reduce parts inventories by using a single cable to provide both power and feedback between drives and motors. And now, operators have more single-cable options at their disposal with the release of new Allen-Bradley 2090 single cables that include halogen-free PUR and PVC options.


Click to download image.

The halogen-free options are ideal for applications like food and beverage, where users want to reduce exposure to toxins, and for applications looking to meet IEC 60754-1.

The cables are designed for systems that use Kinetix 5500 and 5700 servo drives, Kinetix VP-Series servo motors and Kinetix VPAR electric cylinders. The cables also have a smaller bend radius for continuous-flex and static applications and are available in a wide range of cable AWGs, types and connector options.

Allen-Bradley and Kinetix are trademarks of Rockwell Automation Inc.




Published January 29, 2020


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left New PUR and PVC Single-Cable Options Ease Installation, Maintenance