Synchronize the Redundant Chassis Pair

For details about the Synchronize Secondary and Initiate Switchover commands that are used in this procedure, see Initiate Redundancy Commands in the RMCT.
To synchronize the redundant chassis pair after the firmware in both chassis have been updated to the same revision, complete these steps.
  1. Access the RMCT for the redundancy module in the primary chassis.
  2. On the Synchronization tab, select Synchronize Secondary.
    Synchronize Secondary button
  3. When the following warning appears, select Yes to proceed.
    Synchronization warning message
  4. Wait for the synchronization to complete.
  5. If the rotary switches on the communication modules in the redundant chassis are set between 2…254, complete these steps.
    1. Initiate a switchover.
      Initiate Switchover button
    2. In the new secondary chassis, set the rotary switches on the communication modules back to the original configuration.
    3. Repeat this process for all communication modules that need the rotary switches set back to 2…254.
    4. Set Auto-synchronization to your preferred setting.
    5. If you set Auto-synchronization to Conditional, manually synchronize the chassis.
      Synchronize Secondary button
  6. Set the redundancy module date and time according to your preference.
  7. Select Apply.
  8. Close the RMCT.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal