Set the Date and Time via the RMCT

In the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT), you can set the date and time for the redundancy module.
  1. Access the RMCT.
  2. Select the Configuration tab.
  3. In the Redundancy Module Date and Time area, set the time by using one of these methods:
    • Manually select the current date, current time, and date format, and then select Set.
    • Select Apply Workstation Time to use the date and time of the workstation.
    Redundancy Module Date and Time
  4. When the following message appears, select Yes.
    Change Redundancy Module Date and Time Message Confirmation
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal