Connect to Remote I/O
Remote I/O refers to I/O modules that are not in the local chassis and connect to the controller via a communication network. There are several families of I/O modules that are remote from the controller:
- Compact 5000® I/Omodules in a remote bank using a 5069-AEN2TR or similar adapter
- 1756 I/O in a remote chassis via a Network Bridge Module
- Distributed I/O families such as 5034PointMax®I/O or 5094FLEX 5000®I/O.
- On-Machine™I/O families such asArmorBlock®I/O
The controller supports the use of remote I/O via these networks:
- EtherNet/IP™
- ControlNet®
- DeviceNet®
- Universal remote I/O
Provide Feedback