Use the Status Indicators for Troubleshooting

Use the Status Indicators for Troubleshooting

PointMax I/O modules use the following status indicators:
  • SA Power Indicator – This indicator operates the same for all PointMax I/O modules.
  • Module Status Indicator – This indicator operates the same for all PointMax I/O modules.
  • Channel Status Indicator – This indicator operates differently based on the module type you are using.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal