Axisxx – Brake View
Use Axisxx – Brake to view or configure the brake parameters of the specific axis.
Axisxx – Brake View Example

The Axisxx – Brake view includes these parameters:
Parameter | Description |
|---|---|
Disengage Delay Time | Specifies the delay time from axis power turned on until the
brake is released. Valid values are 0…1000 ms |
Engage Delay Time | Specifies the delay time from axis power turned off until the
brake is applied. Valid values are 0…1000 ms |
Provide Feedback