Data Rate
The buad rate is the communication rate (bits per seconds) between the SSI sensor and the
module's SSI channel. The baud rate selected at the SSI channel equals the frequency of
the SSI channel’s clock output. You can configure the Baud rate in Module Properties →
SSI.
The maximum baud rate that can be used for your application is limited by the
transmission line length between the SSI module and sensor. See the SSI sensor data
sheet, as well as the PointMax I/O Specifications Technical Data, publication 5034-TD001, for communication rate versus
transmission line length information.
The time between successive SSI words can be configured in Module Properties → SSI → SSI
Word Delay Time.
See the SSI sensor data sheet for the recommended delay time. If the sensor manufacturer
specifies a value called monoflop time, use that value for the SSI Word Delay time
setting.
The Baud Rate multiplied by Word Length and SSI Word Delay determines the data rate of
SSI channel before filter is applied.
Provide Feedback