Data Format
The SSI sensor data is produced in the
I.SSIxx.Data
tag.If the type of SSI sensor is Binary, the data format is always Binary. If the type of SSI
sensor is Gray code, the displayed data format is always converted from Gray to
Binary.
Some SSI sensor has non-position trailing bits on the data returned. This can be
truncated by configuring the number of Trailing Bits in Module Properties → SSI –
Conversion. This is important to achieve the correct direction and window comparison
result.
If the trailing bits has important information such as status information, the
I.SSIxx.RawData
tag can be used to readback this information. The RawData
contains the data received from the SSI sensor without any conversion or truncation. The
RawData size matches the word length.Provide Feedback